Other Parts Discussed in Thread: TMP1075, , TCA9517A, TCA9509, TCA9617B, TCA9511A, TCA4307, TCA39416, TCA9406, TCA9416
Hello community,
We have to interface 4 to 5 x TMP1075 sensors with our MCU over a maximum bus length of 5m. This shall be a CAT6 UTP cable with SDA & SCL paired with ground wires.
Kindly suggest if there are any 5.5V version with fall slew rate control as an alternative for the TCA9803. Objective is to utilize relatively higher noise margin offered by 5V bus voltage than 3.3V offered by TCA9803.
The clock signal in this case is a maximum of 2kHz.