This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042HGV-Q1: STM32F405 support for TCAN1042HGV-Q1

Part Number: TCAN1042HGV-Q1
Other Parts Discussed in Thread: TCAN1042-Q1

Hi, I'm using TCAN1042HGV-Q1 can IC in my reference design, in which I'm using STM32F405R, can you please confirm me that this can IC is supported by MCU

Thanks 

  • Saket,

    As long as the logic levels meet the thresholds necessary for the TXD and RXD pins on the TCAN1042HGV-Q1, then the MCU will be able to communicate with the CAN channel. Is there a reason the TCAN1042-Q1 is being used? The TCAN1044AV-Q1 has the same pinout and functionality, with better availability, so unless the high voltage rating is needed that comes with the H-version, I'd recommend choosing the TCAN1044AV-Q1.

    Regards,

    Eric Hackett