Part Number: SN65HVD230
Hi Team
Customer is using CAN transceiver SN65HVD230 encountered the problem, bus failure rate is relatively high.
The scenario is: 500K baud rate, the 8-pin RS is pulled down to ground by 20KΩ, the CAN bus is easy to be interference, the failure rate is more than 1%, and the report CRC incorrect. After pulling pin 8 down to 0Ω, the failure rate is significantly improved.
So, they would like to ask if you has encountered similar problems. and
- 1. When the RS pin is pulled down to the ground, why does it have an anti-interference effect?
- 2. what's the root cause of the failure caused by RS using 20K pull-down ?
- 3. When RS is pulled down to the ground, what precautions should be taken when applying it?