Part Number: TPD4S311
Hi,
The typical OVP of TPD4S311 is 6V, the actual use of VBUS by customers will not exceed 5.5V, but the short circuit between 5.5V and CC pin will damage the load chip IO (load chip IO the maximum voltage of the CC pin is 4.02V).
At that time, the original intention of choosing this chip is to improve the protection level to 20V, but the VBUS at 5V, the chip can not play a protective role, is there a similar chip that can start to play a protective role on VBUS5V?
Thanks~