This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CF386: Can I get the 13.5MHz frequency at output side of this part.

Part Number: DS90CF386


Hi Team,

I am using DS90CF386MTD receiver in my designing in which input is coming from CPU and the output is going to FPGA for the resolution 768 x 576 with 50Hz frequency. my requirement is the output clock  RxCLKOUT shoud be 13.5 MHz.

Can I get the same frequency at output side of this part. if yes then then what frequency I should apply at the input side for the same resolution.

also elaborate the function of PLL in receiver only.

I have gone through many designs' application, but I did not get any answer on this.

so please guide us for the same , waiting for your reply.

 Regards,

Sanjay