Please recommend parts :Suppressor for RS485(SOD323 package or smaller package)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For RS-485, we typically recommend ESDS552 but this is in a SOT-23 package which is bigger than what you want. Another device we recommend is ESD752 which is in a SOD323 package. What voltage are you looking for? We do offer smaller packages but those tend to be at lower voltages.
Please let me know if you have additional questions.
Best Regards,
McKenzie Eaker
Hi,
For automotive, we don't have an automotive version of ESDS552 which is 12V in our portfolio currently. But for 24V, there are more options. There is ESD1LIN24-Q1, ESD751-Q1, and ESD761-Q1 which are all SOD323 or smaller and the main difference between them are surge current and ESD rating. We also have a 9V device, TPD1E10B09-Q1 in DFN-1006.
Please let me know if you need a lower voltage device or have additional questions.
Best Regards,
McKenzie