Part Number: TCAN1043A-Q1
Hello team,
We need CAN FD transceiver with wake function which supports 1.8V VIO. I found TCAN1043A-Q1 datasheet which says it supports 1.8V VIO as per below screenshot but all the electrical parameters are given for condition VIO=3.3V (as per below screenshot) and also the lower limit of VIO is 1.7V. So I need confirmation that, whether this transceiver can be used for applications with 1.8V VIO completely.



Thank you in advance
Kavana H