Part Number: SN65HVD234
Application + Implementation
We have designed a product that has two units - a base station and a hand held probe, which communicate with each other using a CAN interface. Both units have SN65HVD234D (or 235) CAN transceivers and T24CAN TVS protection. They are physically connected via a 4 wire curly cable (0V, 12V, CANH, CANL) which is user-detachable. There are no other devices on the CAN Bus.
Customers are now returning the product due to failure of the SN65HVD234D in the hand held probe. We are unable to replicate this fault without implausible abuse and need help to rectify the problem. About 4% of shipped product is affected.
The product is a high voltage breakdown detector, with the hand held probe generating up to 40kV.
Field Returns
- T24CAN TVS parts are intact and functional.
- There are no signs of PCB assembly faults.
- In most cases the IC partially works but the R pin is stuck high.
- In one case the MCU pin connected to transceiver D pin was damaged.
- Half a dozen transceivers have craters, most have signs of heating in conformal coating.
- We have had issues with the 4 way connecting cable failing partially open but it does not appear correlated with transceiver failure.
- We have had failures on transceivers from two different suppliers.
- Two MCU types (Renesas and NXP) are in use, both configurations have had transceiver failures.
- The failures are clustered; some customers have experienced multiple failures.
Tests
All testing has been on the hand-held probe where the failures occur. The transceiver is fed from its own SMPS (== 3V3CAN) while the MCU is fed from a separate low noise LDO. We have tested for the possibility of power sequencing latchup but cannot induce it nor does it fit the evidence or datasheet Fig 28.
Taking 3V3CAN above ~7V causes the transceiver to malfunction but it can recover. Taking 3V3CAN above ~10V causes failure. We are now sending units out with a 3W 4V7 zener (6.1V @ 1.5A) across 3V3CAN and they still fail.
We have tried raising the 12V unit supply to 30V but both regulators take it without complaint. Although it is possible to damage the transceiver with excess voltage on R/D, we do not think this is occurring.
We have tried shorting 12V (and up to 24V) to CANH and CANL, even with D pin stuck low (forced dominant). The thermal protection functions as expected.
We have tried applying transients of 32V PSU and up to 40kV from the HV end of the probe (~50pF, 2uC, 40mJ) without any problems.
We have tried operating the unit with faulty interconnecting cable and without equipment safety ground.
Any help would be gratefully received,
Mike Page.