Part Number: SN75LVPE4410
It's a relate question to SN75LVPE4410: what is the function of reg_06 Register drv_eq_en_override ? - Interface forum - Interface - TI E2E support forums
We are using SN75LVPE4410 under a non PCI-e condition. And set the chip RXDET pin with a 59kOhm resistor.
But we find that output amplitude become bigger when setting "drv_eq_en_override" bit on of reg_06 Register.
Will this receiver detect state machine setting also influenced the output amplitude?
If not, how could we set the chip using PIN mode to have the same amplitude comparing to I2C mode?