Part Number: SN65DPHY440SS
Hello team
I like to use a 500mm cable between the processor and the display. Using a high quality TwinAx cable from 3M the insertion loss is <5dB at the desired frequency and can be compensated by the SN65DPHY440SS. However the MIPI D-PHY specification V1.1 notes a maximal flight time of 2 ns that can obviously not be compensated.

Is the return channel of the display still functional even with the higher round trip time caused by the cable?
Considering the SN65DPHY440SS has a delay of >12 ns on it's own how can the chip be compliant with MIPI D-PHY V1.1 in the first place as it violates the flight time requirement?
Thanks for clarification
Best regards
Stefan