Part Number: DP83867ERGZ-R-EVM
Hi,
I have a quick question about the DP83867ERGZ-R-EVM board. Here is out test setup. The interface between the Soc Dev Board and DP83867ERGZ-R-EVM is RGMII.
SoC Dev Board ---------- DP83867ERGZ-R-EVM ---------- Router ---------- Test PC
The PHY link is established at 1000Mbps/Full duplex successfully. Both LED_0 and LED_1 on the EVM board light up. When the Test PC sends pings to the board, the LED_2 keeps blinking, but the RX_DATA/RX_CTRL signals are NOT toggling.
My question is, if we disconnect the Soc Dev Board from the EVM board, and then keep sending pings from the Test PC to the DP83867ERGZ-R-EVM board, are we supposed to see the RX_DATA and RX_CTRL signals toggling?
Thanks,
Amy