Part Number: TUSB321AI
Other Parts Discussed in Thread: TUSB321
Hi Team,
We are using TUSB321A in one of our projects.
I'm using the TUSB321A as DFP configured according to the spec and the current mode is set to the Default current mode.
I'm using Type-C to Type-A converter.
The problem statement is One way in Type-C is detecting USB3.0 but the other way in Type-C is not able to detect USB3.0.
CC2 is going low to 0.42V (i,e: It is within its Threshold limit) when USB3.0 device connected and DIR pin also going high hence USB3.0 device is detected in terminal.
CC1 is going low to 0.7V(i,e: It is not within its Threshold limit) when USB 3.0 device connected, and the DIR pin is not going low and hence the USB3.0 device is not detected.
Request you to provide us a breakthrough from this.
Hereby attaching the snapshot of the schematic and the scope shots of CC1 & CC2 w.r.t DIR pin for your reference.
Thanks.