Part Number: SN65HVD1476
Is it possible to configure RS485 in a multi-master setup with full-duplex communication using the SN65HVD1476?
If so, How do I configuration it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD1476
Is it possible to configure RS485 in a multi-master setup with full-duplex communication using the SN65HVD1476?
If so, How do I configuration it?
Hi Jooin,
As Clemen's pointed out. The SN65HVD1476 is an transceiver only(helps to redrive the data using fully differential signals across cables).
The device itself can drive a signal through a cable (driver) on one channel and can receive a fully differential signal (receiver) on a completely different channel. You can set up your system to use each channel to send data and receive data at the same time using the two different channels.
-Bobby