Other Parts Discussed in Thread: TUSB1002A, TUSB501,
I have a problem with signal quality in a USB3 device and tested the SN65LVPE512EVM eval board which surprisingly solved all the issues with the default settings.
Unfortunately it does not work when increasing the Equalization and all alternative circuits I have found have at least +3dB EQ.
Is there an alternative which is possible to set to 0dB EQ and 0dB DeEmphasis?
As this chip is not recommended for future designs, is there a time schedule for when it will be unavailable to buy?
Regards
Björn