Other Parts Discussed in Thread: SN75LVDS83B, TFP403, SN65DSI85, DS90C387, TFP410, DS90CR218A, DS90CF366, DS90CR486, DS90CR484A, DS90CF388
I've just registered and this is my first post - a little about me at the end.
I am hoping to prototype a quite basic picture monitor for high-end applications. A picture monitor differs from a TV in that it has no provision for audio and does not include a tuner; it differs from a computer monitor in that it is designed to accept a video format rather than a PC format signal. In CRT technology, picture monitors were designed to add nothing to, or take anything away from, the signals fed to them and used bespoke high resolution CRTs - often with the original delta gun arrangement - and (in Europe) the correct "EBU" phosphors for accurate colorimetry.
My LCD picture monitor would be used with a Lumagen Radiance XE 10-bit video processor which would act as a switcher, take care of deinterlacing of interlaced inputs, upscale standard definition inputs, manage colour and gamma - and always output 1920 x 1080 progressive at 50Hz on HDMI.
I am still to choose my LCD panel - I am looking for: 32 inch : 1920 x 1080 : 50Hz : 10-bit : S-IPS or AS-IPS. I still have some research to do regarding refresh rate and number of bits. To preserve picture quality I want to avoid frame-rate conversion and work at 50Hz throughout, but the video processor can convert to 60Hz if I have to work 60Hz. I'm not sure if true 10-bit (total: 30 bits) panels are available - it seems many 10-bit panels are actually dithered 8-bit (total: 24 bits) panels. There are two products - a Sony LMD3250MD 32" medical grade monitor and an Ikegami HLM-3250W 32" broadcast grade monitor - which claim to use 10-bit panels which I am investigating.
So, in principle, this is a straightforward task and, once I've chosen my LCD panel, all I need is a means of converting the HDMI signal from the Lumagen Radiance XE video processor to the (multi-port) LVDS signals required by the panel. I'm not sure yet whether the converter will need a control interface but think this is likely as with ICS's NT15H LCD Controller Board and multi-button NK05A OSD Control Board - see http://www.icsco.kr/what_we_serve/sub_02.asp
So, to summarise I need:
- HDMI or DVI-D (dual-link) input
- 1920 x 1080 at 50Hz operation (option: 60Hz)
- Multi-port LVDS output
Can't be that difficult... can it?
About me: I'm a semi-retired, degree-qualified electronics engineer - I graduated from Imperial College, London in 1979 and then joined BBC TV where I worked as an engineer in their London television studios on the full range of broadcast equipment and have some 30 years' experience designing, building, repairing and modifying professional and consumer electronics. In 1987 I moved to Channel 4 TV, London where I worked until 2006, at the end as manager of the team of engineers which kept the transmission operations running.