Part Number: DP83822IF
Hi Support Team,
DP83822IF In FX mode, when plugging and unplugging with traffic, the link cannot be established.
Is there a register or method that can solve this problem?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83822IF
Hi Support Team,
DP83822IF In FX mode, when plugging and unplugging with traffic, the link cannot be established.
Is there a register or method that can solve this problem?
Thanks.
Hi Ryan!
I understand your predicament quite well. There is a note in Section 8.4.4.2 100Base-FX Receive of the data sheet describing this issue, as well as an FAQ that I have linked below.
Basically, this is a known issue with the DP83822. The link status won't change in fiber, in order to get the correct link status, a soft-reset must be performed (Set Reg 0x1F = 0x4000) before reading Register 0x1.

Regards,
Alvaro