This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1310: TUSB1310 IBIS AMI model

Part Number: TUSB1310


Hi, how can I find the IBIS AMI model of TUSB1310 which is a USB 3.0 transceiver. I need this model to use in Hyperlynx simulation. I guess TUSB1310 is quite old device and support up to 5 Gbps. Do we have any newer version of the USB 3.0 transceiver that support 10 Gbps ? If yes, how can I get their IBIS AMI models ?