Part Number: DS90UB662-Q1
Hi team,
Hope you are doing well!
I have two CSI2 bandwidth calculation tools, V2.2 and V2.3, but the calculation results are not consistent, so I am not sure whether I can use DS90UB662-Q1.
1. This is the calculation result of V2.2, 1.7G per camera, so 662 cannot support

2. This is the calculation result of V2.3. 1.47G per camera, so 662 can support

So, why they are different? Even if Blanking 25% in V2.2 is removed, it is still different.