Part Number: TCAN1145-Q1
Can you confirm whether it is possible to configure multiple CAN messages as the wakeup frames in this transceiver?
MPN: TCAN1145-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1145-Q1
Can you confirm whether it is possible to configure multiple CAN messages as the wakeup frames in this transceiver?
MPN: TCAN1145-Q1
Hi Pratik,
The TCAN1145 supports multiple wake IDs and data byte configurations through the use of masks on both the ID and data component of the wake up frame. This allows a range of IDs to be used based on maskable bits, though not any combination of IDs / Data may be used or excluded.
Let me know if this is clear and if you have any more questions.
Regards,
Eric Schott