Part Number: DP83TC812EVM-MC
I have connected a DP83TC812EVM and a DP83TC813EVM as shown in the following figure. I have adjusted the MDIO addresses by removing the resistors as follows to get by with only one USB connection:
- DP83TC812 on DP83TC812EVM = 10
- DP83867 on DP83TC812EVM = 1
- DP83TC813 on DP83TC813EVM = 0
- DP83867 on DP83TC813EVM = 3
The power is supplied via USB.
Now let's talk about my problem:
- A ping via this connection is not possible. (if only the ethernet ports are connected, the ping works, so it cannot be due to a firewall)
- If the DP83TC812EVM register 0624 is set to 55BF and 0619 to 1555 via MDIO, there seems to be a data stream via the SPE connection. The LED1 of the DP83TC812EVM flashes and the LED of the Ethernet port also flashes. However, no packets can be detected using the network sniffing tool (Wireshark).
What could be the reason for this? I have already checked the registers of the DP83867 and they should actually fit like this.