Part Number: TCA9535
Other Parts Discussed in Thread: TCA6507
Hi team,
could TCA9535 be configured with a 110Hz PWM output (just need a simple square pulse)?
Regards
SK Loo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TCA9535 has no internal clock. You would have to switch the output pin manually from the I²C master. At 400 kHz, one write transaction would need about 70 µs, so this would, in theory, be possible.
It would be much easier to do this with a microcontroller's PWM output pin.
SK,
Like Clemens stated, no internal clock present that would allow configurability for PWM duty cycle. What Clemens is suggested is to constantly write to the IO expander device by turning ON/OFF output ports to make a psuedo PWM waveform on the p-port side. 110Hz seems possible with this method of repeated i2c writes to the expander.
Either MCU PWM output pin is way easier, and will not take up as much bandwidth on the I2C bus using this method.
Consider TCA6507 for configurable PWM outputs. This would also save much bandwidth on the i2c bus.
Regards,
Tyler