Part Number: DS125BR111
Hello,
I'm looking at the data for DS125BR111RTWR. I see that the part is rated only to -40°C for low operating/storage temperature. This part was apparently tested to -65°C during temperature cycling. I had two questions here:
1) in one of the row it says "Temperature cycle -65/150C ..... Or equivalent JEDEC condition", would this be considered test condition "C" since that is its equivalent. I just want to verify what testing was done and that it isn't something less than what is is the conditions column
2) Is there any reason why this part couldn't be stored at a lower temperature than the -40°C. Such as material expansion differences, some internal construction that would fail, anything? If the part has been temperature cycled to -65°C I'd figure I could use some engineering judgement and say it could be stored lower.
Thank you,
Trace