This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem Communicating CC430 with AT24C1024

Hello,

I was testing I2C operation between two development boards(EM430F5137RF900) using sample codes.

I could successfully make the I2C work.

But when i'm trying to communicate with an EEPROM (AT24C1024 From Atmel)  i can't detect the ACK from the EEprom.

MY I2C Clock is almost 540 KHz

E2PROM Datasheet:

http://www.atmel.org/dyn/resources/prod_documents/doc1471.pdf

 

Here is My Code:

SMCLK is  8Mhz

 

void I2C_Init(void)
{
 //..........
 
// ACLK = REFO = 32kHz, MCLK = SMCLK = 8MHz//
  /* Initialize Ports */
 
  PMAPPWD = 0x02D52;                                        // Get write-access to port mapping regs 
  P2MAP0 = PM_ACLK;                                          // Map ACLK output to P2.0
  P2MAP2 = PM_MCLK;                                         // Map MCLK output to P2.2
  P2MAP4 = PM_SMCLK;                                      // Map SMCLK output to P2.4
  PMAPPWD = 0;                                                     // Lock port mapping registers 
  
  P2DIR |= BIT0 + BIT2 + BIT4;                            // ACLK, MCLK, SMCLK set out to pins
  P2SEL |= BIT0 + BIT2 + BIT4;                           // P2.0,2,4 for debugging purposes

  UCSCTL3 |= SELREF_2;                                  // Set DCO FLL reference = REFO
  UCSCTL4 |= SELA_2;                                        // Set ACLK = REFO

  __bis_SR_register(SCG0);                             // Disable the FLL control loop
  UCSCTL0 = 0x0000;                                         // Set lowest possible DCOx, MODx
  UCSCTL1 = DCORSEL_5;                              // Select DCO range 16MHz operation
  UCSCTL2 = FLLD_1 + 249;                            // Set DCO Multiplier for 8MHz
                                                                                // (N + 1) * FLLRef = Fdco
                                                                                // (249 + 1) * 32768 = 8MHz
                                                                                // Set FLL Div = fDCOCLK/2
  __bic_SR_register(SCG0);                             // Enable the FLL control loop

                                                                                // Worst-case settling time for the DCO when the DCO range bits have been
                                                                                // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
                                                                                // UG for optimization.
                                                                                // 32 x 32 x 8 MHz / 32,768 Hz = 250000 = MCLK cycles for DCO to settle
  __delay_cycles(250000);

 //............................
 
 PMAPPWD = 0x02D52;                       
 P1MAP3 = PM_UCB0SDA;                    
 
 P1MAP2 = PM_UCB0SCL;                    
 PMAPPWD = 0;                             
 P1SEL |= (BIT2+BIT3);
 //............................
 UCB0CTL1 |= UCSWRST;                                                  // Enable SW reset
 UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC ;        // I2C Master, synchronous mode
 UCB0CTL1 = 0xC0 + UCTR + UCSWRST ;                     // Use ACLK, keep SW reset
 UCB0BR0 = 12;
 UCB0BR1 = 0x00;
 UCB0I2CSA = 0xA0;                                                            // E2Prom Address
 
// UCB0I2COA=0x01a5;                                                       //  ----> Master Own Address
 UCB0CTL1 &= ~UCSWRST;

 

Any comment would be appriciated,

Thx