Part Number: TCAN1043-Q1
Other Parts Discussed in Thread: TCAN1043, STRIKE
I work in the automotive industry and one of our design includes the TCAN1043A network wake CAN transciever. We're experiencing failures of the devices frequently throughout environmental testing.
Originally in our dual µController design, we used two transceivers. For the INH output of both transceivers we chose 10kΩ (effectively 5kΩ in parallel) as pulldowns. This enabled each transciever to wake both power supply chips (PMIC).
We opened a failure analysis with your quality team with the numbers provided below:
QEM-CCR-2312-00886 CPR231092014
The failure analysis came back with a very much damaged trace to pin (8) nFAULT.
We looked at our design again and the value of the pulldowns drove current higher than the recommended operating conditions of 1mA from the INH pin, but did not exceed the absolute maximum value of 6mA. Regardless, we updated our design by increasing the pulldown resistance on the INH pin to effectively 50k and reducing the maximum current draw to less than 1mA.
Before receiving the results of the FA, we hypothesized that we INH was the likely cause of the failed IC, but the FA results don't specifically support that. Internally to the chip, the INH pin looks like it runs very close to the nFAULT damage and am looking for someone to discuss if there is a link to our design flaw and the failed nFAULT pin.
I tried to add an image of our design and failure analysis, but the resolution made it semi-illegible.