Other Parts Discussed in Thread: TPS25762-Q1, TPS25730
Hi, TI expert
The customer is currently reviewing the development of the LTE Tracker.
Below is the block diagram of the power section of the product under review.
The customer is looking for a USB PD controller in the block diagram above.
I want to read data and charge the built-in battery through the USB Type-C connector. (Battery: Lithium Polymer, 3000mAh, 1C, 1-cell)
According to what I checked on TI.com, it is about TPS25762-Q1 (TPS25762-Q1 data sheet, product information and support | TI.com), and it is an Automotive product.
Is TPS25762-Q1 also suitable?
Is there a USB PD controller that can be recommended as a Non-Auto product? (CC pin must be present)
Please check. Thank you.