This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: SGMII_to_RGMII bridge mode link up succeed, but fail to transmission data

Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869,

Dear,

 One customer who is from Nvidia used DP83869 for his application and met the following  question:

[

I choose DP83869 to connect SGMII mac with RGMII phy. After pulling up PIN_22 GPIO_1, PIN_36 RX_D3 and PIN_38 RX_CTRL(SGMII_to_RGMII bridge mode), they can link up in 1000M_FULL mode and SGMII mac can receive data from RGMII phy. But RGMII phy cannot  receive data from SGMII mac.

It's even more confusing that if PIN_38 RX_CTRL pull-up is broken the performance of this system is consistent with the above which is supposed to be RGMII_to_SGMII bridge mode.

Because of design error, I cannot get the information of the registers in DP83869HM. I don't know how to find out where the problem lies and wish to get help from you.}]

Best regards

Kailyn