Part Number: TPD4E05U06
Dear Specislists,
My customer is considering TPD4E05U06 for 10/100 Ethernet protection.
They have a question.
I would be grateful if you could advise.
---
According to the datasheet of P.4 Table 5-2, Pins 6, 7, 9, and 10 are NC pins and should be connected to left open or GND.
On the other hand, the circuit diagram of "DP83822 EVM", it is connected to RXD and TXD.
https://www.ti.com/lit/pdf/snlu179

Which connection is correct?
I am thinking as stated in the data sheet, pins 6, 7, 9, and 10 are unconnected (NC) or GND , and IO is 1, 2, 4 and 5 pin,
Is there any problem with a circuit that connects to pin 5 and pins 3 and 8 to open or GND?
---
I appreciate your great help in advance.
Best regards,
Shinichi