This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640: PTP_TDR register information

Part Number: DP83640

I am trying to find certain information in datasheet for PTP_TDR (page 4), but with no luck.

I am using the dp83640 April 2015 datasheet.

In paragraph  5.6.1.5.2 it is indicated:

"On Writes, successively stores the 16-bit values of Clock time or Trigger Control
Information as selected by controls in the PTP Control Register."

However, I can't find anywhere information about which are the successive stores from Clock time or Trigger Control.

Related to that, in the software development guide I see:

EXPORT void
    PTPArmTrigger (
        IN PEPL_PORT_HANDLE portHandle,
        IN NS_UINT trigger,
        IN NS_UINT32 expireTimeSeconds,
        IN NS_UINT32 expireTimeNanoSeconds,
        IN NS_BOOL initialStateFlag,
        IN NS_BOOL waitForRolloverFlag,
        IN NS_UINT32 pulseWidth,
        IN NS_UINT32 pulseWidth2)

//  Establishes a trigger's expiration time and trigger pulse width behavior.
//  
//  portHandle
//      Handle that represents a port. This is obtained using the EPLEnumPort 
//      function.
//  trigger
//      The trigger to arm, 0 - 7.
//  expireTimeSeconds
//      The seconds portion of the desired expiration time relative to the 
//      IEEE 1588 hardware clock. 
//  expireTimeNanoSeconds
//      The nanoseconds portion of the desired expiration time relative to 
//      the IEEE 1588 hardware clock. This value may be not be larger then 
//      1e9 (1 second).
//  initialStateFlag
//      Indicates initial state of signal to be set when trigger is armed 
//      (FALSE will cause a signal rise at trigger time, TRUE will cause a 
//      signal fall at trigger time). This parameter is ignored in toggle 
//      mode.
//  waitForRolloverFlag
//      If set to TRUE the device should not arm the trigger until after 
//      the seconds field of the clock time has rolled over from 
//      0xFFFF_FFFF to 0.
//  pulseWidth
//      Sets the 50% duty cycle time for triggers 2 - 7. Its format is 
//      bits [31:30] = seconds, [29:0] = nanoseconds. For triggers 0 and 1 
//      sets the width of the first part of the pulse, the width of the 
//      second part of the pulse is set by the pulseWidth2 parameter.
//  pulseWidth2
//      Ignored for triggers 2 - 7. For Triggers 0 and 1, in a single or 
//      periodic pulse type signal, a second pulse width value controls the 
//      2nd pulse width (period is pulseWidth + pulseWidth2). 
//      Its format is bits [31:30] = seconds, [29:0] = nanoseconds.
//
//      For Edge type signals, pulseWidth2 is interpreted as a 16-bit seconds 
//      field and pulseWidth is a 30-bit nanoseconds field. 
//
//  Returns
//      Nothing
//
//  Once this function has been called, the trigger will be armed. 
//****************************************************************************
{
NS_UINT reg;

    OAIBeginMultiCriticalSection( portHandle->oaiDevHandle);
    reg = (trigger << P640_TRIG_SEL_SHIFT) | P640_TRIG_LOAD;
    EPLWriteReg( portHandle, PHY_PG4_PTP_CTL, reg);
    
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, expireTimeNanoSeconds & 0xFFFF);
    
    reg = (expireTimeNanoSeconds >> 16) | (initialStateFlag ? 0x80000000 : 0) |
          (waitForRolloverFlag ? 0x40000000 : 0);
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, reg);
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, expireTimeSeconds & 0xFFFF);
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, expireTimeSeconds >> 16);
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, pulseWidth & 0xFFFF);
    EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, pulseWidth >> 16);
    
    if ( trigger <= 1)
    {
        EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, pulseWidth2 & 0xFFFF);
        EPLWriteReg( portHandle, PHY_PG4_PTP_TDR, pulseWidth2 >> 16);
    }
    
    reg = (trigger << P640_TRIG_SEL_SHIFT) | P640_TRIG_EN;
    EPLWriteReg( portHandle, PHY_PG4_PTP_CTL, reg);
    OAIEndMultiCriticalSection( portHandle->oaiDevHandle);
    return;
}

I can't find in the datasheet these consecutive data fields that are written in PTP_TDR.

Moreover, the above PTPArmTrigger method has a variable name expireTimeSeconds. However, in the example of the software development guide this variable is named ppsStartTime.

        PTPArmTrigger( portHandle, 0, ptpStackCfg->ppsStartTime, 0, 
                       ptpStackCfg->ppsRiseOrFallFlag, FALSE, 500000000, 500000000);

Which of the two holds? Is it a start time or expiring time?

  • Hi George,

    Thank you for the query.

    Please expect a follow-up by Tuesday 2/6.

    Regards,

    Evan

  • Hi George,

    From my understanding, all 16 bits of 0x15 are reserved for clock time / trigger control information (depending on control setting in 0x14), and writing to 0x15 will store the most recent value for the next read.

    I see the conflict between the variable and method naming. Please treat this as the desired expiration time relative to the hardware clock.

    Thank you,

    Evan

  • Hi Evan,

    I am adding some information I found for anyone interested in the future.

    The sequence of information required to be written for the Clock time or Trigger Control can be found in the Software Development Guide under the section "IEEE 1588 Triggers".

    Regarding the conflicting naming, I still find the term expiring a bit confusing. From my experiments this variable looks like the start time of the trigger relative to the hardware clock.