Part Number: HD3SS3212
Can I use HD3SS3212 to switch Aurora (Xlinx fast Transcivers - like CML) at 10Gbps or 6.25Gbps?
If it possible, can you suggest how connect HD3SS3212 to FPGA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3212
Can I use HD3SS3212 to switch Aurora (Xlinx fast Transcivers - like CML) at 10Gbps or 6.25Gbps?
If it possible, can you suggest how connect HD3SS3212 to FPGA
Hi Lioz,
Could you give more detail on the signal characteristics? This device can pass 10Gbps so the signal speed is ok, but there are a few other considerations to make:
- Is the signal single ended or differential? The 3212 is designed for differential signals and may not be a good solution for single ended.
- What common mode voltage would the signal have? The 3212 can support common mode voltages from 0 to 2V.
- What is the amplitude of the signal? The 3212 can support up to 1.8V differential Vpp

Best,
Shane
signal definition by Xlinx
The Aurora 8B/10B protocol uses differential signaling between ports. This section
specifies signals using peak-to-peak differential voltages. . Each signal swings between A volts and B volts. Using these waveforms, the
definitions are as follows:
1. The transmitter or receiver has a peak-to-peak range of A - B
2. The differential signal ranges from +|A−B| to -|A-B|
3. The differential peak-to-peak signal is 2 * (A−B)
Peak-to-peak is the difference between the most positive and the most negative
readings of a particular signal. In this case (A−B) −(−(A−B)) = 2*(A−B).
To illustrate this concept using real values, consider the case where a current mode logic
(CML) transmitter has a termination voltage of 2.5V and has a swing between 2.5V and
2.0V. Using these values, the peak-to-peak range is 500 mV. The differential signal ranges
between 500 mV and -500 mV. The peak differential signal is 500 mV. The differential peakto-
peak signal is 1000 mV.
Hi Lioz,
If the differential Vpp is 1000mV as you've described then this device should be ok to use.
Be sure that the common mode voltage of your signal is within 0 - 2V. If it is not, you would need to AC couple the MUX.
can you suggest how connect HD3SS3212 to FPGA
I'm not entirely sure what you mean here. The HD3SS3212 is a 2:1 MUX with the signal paths shown below.

If you route signals through in this fashion then there shouldn't be an issue.
Best,
Shane