Part Number: DS90UB934-Q1
Hi TI Experts,
Do you have the python script for the MAP test of DS90UB934 and DS90UB933?
We want to use MAP test to check the quality of our transmission lines.
Thank you!
Regards,,
HJ.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB934-Q1
Hi TI Experts,
Do you have the python script for the MAP test of DS90UB934 and DS90UB933?
We want to use MAP test to check the quality of our transmission lines.
Thank you!
Regards,,
HJ.
Hi HJ,
Yes, when downloading Analog LaunchPAD, predefined example scripts will be available in the file directory, which includes a 934 Margin Analysis script. The example file path location is shown here: C:\Program Files (x86)\Texas Instruments\Analog LaunchPAD v1.57.0010\PreDefScripts\DS90UB934\ub934_margin_analysis_script
I've attached the script to this E2E for reference as well.
"""
Copyright 2018 Texas Instruments Incorporated. All rights reserved.
IMPORTANT: Your use of this Software is limited to those specific rights
granted under the terms of a software license agreement between the user who
downloaded the software, his/her employer (which must be your employer) and
Texas Instruments Incorporated (the "License"). You may not use this Software
unless you agree to abide by the terms of the License. The License limits your
use, and you acknowledge, that the Software may not be modified, copied or
distributed unless embedded on a Texas Instruments microcontroller which is
integrated into your product. Other than for the foregoing purpose, you may
not use, reproduce, copy, prepare derivative works of, modify, distribute,
perform, display or sell this Software and/or its documentation for any
purpose.
YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
PROVIDED AS IS WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL TEXAS
INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER LEGAL
EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES INCLUDING BUT NOT
LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE OR CONSEQUENTIAL
DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT OF SUBSTITUTE GOODS,
TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES (INCLUDING BUT NOT
LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
Should you have any questions regarding your right to use this Software,
contact Texas Instruments Incorporated at www.TI.com.
"""
# Name: ub934_margin_analysis.py
# Purpose: Margin Analysis Script for DS90UB934
# Version 0.97
# Run from DES
print "\n"
import time
import logging
# Select log file name and log level(DEBUG, INFO)
logging.basicConfig(filename='ub934sfeq_testlog.log', filemode='a', format='%(levelname)s:%(message)s',level=logging.DEBUG)
# Select RX Port: RX_PORT0_934B or RX_PORT1_934B
CONST_RXPORT = 'RX_PORT0_934B'
# configure I2C device ID of the DES per IDX strap pin
# EVM: 0x60, SVB: 0x7A, Custom Board: 0x??
devAddr_DES = 0x60
f1=open('./ub934sfeq_test.csv', 'w+')
f1.write(",,,,,,,,SP,,,,,,,,")
f1.write("\r")
f1.write("EQ,0,1,2,3,4,5,6,7,8,9,10,11,12,13,14")
# default (0x83) is for port0, for port1 would need to change thie to be 0x97.
if CONST_RXPORT == 'RX_PORT0_934B':
#set RX_PORT_CTL register
board.WriteI2C(devAddr_DES,0x0C,0x83)
time.sleep(0.1)
#set FPD3_PORT_SEL register
board.WriteI2C(devAddr_DES,0x4c,0x01)
time.sleep(0.1)
# choose analog register page
board.WriteI2C(devAddr_DES, 0xB0, 0x04)
time.sleep(0.1)
elif CONST_RXPORT == 'RX_PORT1_934B':
#set RX_PORT_CTL register
board.WriteI2C(devAddr_DES, 0x0C, 0x97)
time.sleep(0.1)
#set FPD3_PORT_SEL register
board.WriteI2C(devAddr_DES,0x4c,0x12)
time.sleep(0.1)
# choose analog register page
board.WriteI2C(devAddr_DES, 0xB0, 0x08)
time.sleep(0.1)
else:
#set RX_PORT_CTL register
board.WriteI2C(devAddr_DES,0x0C,0x83)
time.sleep(0.1)
#set FPD3_PORT_SEL register
board.WriteI2C(devAddr_DES,0x4c,0x01)
time.sleep(0.1)
# choose analog register page
board.WriteI2C(devAddr_DES, 0xB0, 0x04)
time.sleep(0.1)
# choose reg_8 @ offset 8
board.WriteI2C(devAddr_DES, 0xB1, 0x08)
time.sleep(0.1)
# configure AEQ_CTL register: Disable SFILTER adaption with AEQ
board.WriteI2C(devAddr_DES, 0x42, 0x70)
time.sleep(0.1)
# set AEQ Bypass register: bypass AEQ, STAGE1=0, STAGE2=0, Lock Mode = 1
board.WriteI2C(devAddr_DES, 0xD4, 0x01)
time.sleep(0.1)
# set Parity Error Threshold Hi Register
board.WriteI2C(devAddr_DES, 0x05, 0x00)
time.sleep(0.1)
# set Parity Error Threshold Lo Register
board.WriteI2C(devAddr_DES, 0x06, 0x01)
time.sleep(0.1)
# Enable Encoder CRC error capability
enc_crc = board.ReadI2C(devAddr_DES, 0x4A, 0x01)
board.WriteI2C(devAddr_DES, 0x4A, (enc_crc | 0x10))
# Enable Encoder CRC
enc_crc = board.ReadI2C(devAddr_DES, 0xBA, 0x01)
board.WriteI2C(devAddr_DES, 0xBA, (enc_crc & 0x7F))
logging.info('**** Begin Initial Settings ****')
logging.info('Test lock status with sfilter changes')
logging.info('Check RX_PORT_CTL Register (0x0C): %s', hex(board.ReadI2C(devAddr_DES, 0x0C, 1)))
logging.info('Select PORT 0 (0x4C): %s', hex(board.ReadI2C(devAddr_DES, 0x4c)))
logging.info('Check RX_PORT_STS1 Register (0x4D): %s', hex(board.ReadI2C(devAddr_DES, 0x4D, 1)))
logging.info('Check Device Status Register (0x04): %s', hex(board.ReadI2C(devAddr_DES, 0x04,1)))
logging.info('Disable sfilter adaption in AEQ_CTL register (0x42): %s', hex(board. ReadI2C(devAddr_DES, 0x42)))
logging.info('Check AEQ_CTL2 register (0xD2): %s', hex(board.ReadI2C(devAddr_DES, 0xD2,1)))
logging.info('Check AEQ MIN/MAX register (0xD5): %s', hex(board.ReadI2C(devAddr_DES, 0xD5,1)))
logging.info('Check AEQ BYPASS register (0xD4): %s', hex(board.ReadI2C(devAddr_DES, 0xD4,1)))
logging.info('reg_8 initial value: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
logging.info('Updated AEQ BYPASS register (0xD4): %s', hex(board.ReadI2C(devAddr_DES, 0xD4,1)))
logging.info('**** End Initial Settings ****')
# delay before lock is checked, use minimum of 0.5 when doing digital reset
dwell_time = 0.9
for y in range(0,1):
eq_sel2 = 0
#eq_sel1 is needed from 0 to 7
for eq_sel1 in range(0, 8, 1):
board.WriteI2C(devAddr_DES, 0xD4, ((eq_sel1<<5)+(eq_sel2<<1)+0x01))
time.sleep(0.1)
logging.debug('AEQ BYPASS register (0xD4): %s', hex(board.ReadI2C(devAddr_DES, 0xD4,1)))
time.sleep(0.1)
logging.info('%s', hex(eq_sel1))
print 'eq_sel1= ', hex(eq_sel1)
print 'lock status:'
f1.write("\r")
out_string = str(eq_sel1) + ","
f1.write(out_string)
ddly_ctrl = 8 #(disable 6 extra delay)
for cdly_ctrl in range(15, 8, -1):
# write reg_8
board.WriteI2C(devAddr_DES, 0xB2, ((ddly_ctrl<<4) + cdly_ctrl))
time.sleep(0.1)
logging.debug('**reg_8 updated value**: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
# reset digital block except registers
board.WriteI2C(devAddr_DES, 0x01, 0x01)
time.sleep(dwell_time)
port_status1 = board.ReadI2C(devAddr_DES, 0x4D,1)
logging.debug('Check RX_PORT_STS1 Register (0x4D): %s', hex(port_status1))
time.sleep(0.1)
logging.debug('port lock status: %s', hex(port_status1 & 0x01))
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E,1)
logging.debug('Check RX_PORT_STS2 Register (0x4E): %s', hex(port_status2))
time.sleep(0.1)
lock_status = 0
lock_sum = 0
for loop in range(0, 10, 1):
port_status1 = board.ReadI2C(devAddr_DES, 0x4D, 1)
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E, 1)
time.sleep(0.1)
if (((port_status1 & 0x3C) == 0) and ((port_status2 & 0x20) == 0)):
lock_sum += int(port_status1 & 0x01)
else:
board.ReadI2C(devAddr_DES, 0x56, 1) # clear parity error
time.sleep(0.1)
lock_avg = round(float(lock_sum) / 10, 2)
lock_str = "%0.1f" %lock_avg
logging.debug('port lock status: %s', lock_str)
time.sleep(0.1)
out_string = lock_str + ","
f1.write(out_string)
print lock_str
logging.debug('**cdly_ctrl value at end of loop**: %s', hex(cdly_ctrl))
cdly_ctrl = 8 #(disable 6 extra delay)
for ddly_ctrl in range(8, 16, 1):
# write reg_8
board.WriteI2C(devAddr_DES, 0xB2, ((ddly_ctrl<<4) + cdly_ctrl))
time.sleep(0.1)
logging.debug('**reg_8 updated value**: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
# reset digital block except registers
board.WriteI2C(devAddr_DES, 0x01, 0x01)
time.sleep(dwell_time)
port_status1 = board.ReadI2C(devAddr_DES, 0x4D,1)
logging.debug('Check RX_PORT_STS1 Register (0x4D): %s', hex(port_status1))
time.sleep(0.1)
logging.debug('port lock status: %s', hex(port_status1 & 0x01))
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E,1)
logging.debug('Check RX_PORT_STS2 Register (0x4E): %s', hex(port_status2))
time.sleep(0.1)
lock_status = 0
lock_sum = 0
for loop in range(0, 10, 1):
port_status1 = board.ReadI2C(devAddr_DES, 0x4D, 1)
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E, 1)
time.sleep(0.1)
if (((port_status1 & 0x3C) == 0) and ((port_status2 & 0x20) == 0)):
lock_sum += int(port_status1 & 0x01)
else:
board.ReadI2C(devAddr_DES, 0x56, 1) # clear parity error
time.sleep(0.1)
lock_avg = round(float(lock_sum) / 10, 2)
lock_str = "%0.1f" %lock_avg
logging.debug('port lock status: %s', lock_str)
time.sleep(0.1)
out_string = lock_str + ","
f1.write(out_string)
print lock_str
eq_sel1 = 7
#eq_sel2 is needed only from 1 to 7
for eq_sel2 in range(1, 8, 1):
board.WriteI2C(devAddr_DES, 0xD4, ((eq_sel1<<5)+(eq_sel2<<1)+0x01))
time.sleep(0.1)
logging.debug('AEQ BYPASS register (0xD4): %s', hex(board.ReadI2C(devAddr_DES, 0xD4,1)))
time.sleep(0.1)
logging.info('%s', hex(eq_sel2))
print 'eq_sel2= ', hex(eq_sel2)
print 'lock status:'
f1.write("\r")
out_string = str(eq_sel1+eq_sel2) + ","
f1.write(out_string)
ddly_ctrl = 8 #(disable 6 extra delay)
for cdly_ctrl in range(15, 8, -1):
# write reg_8
board.WriteI2C(devAddr_DES, 0xB2, ((ddly_ctrl<<4) + cdly_ctrl))
time.sleep(0.1)
logging.debug('**reg_8 updated value**: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
# reset digital block except registers
board.WriteI2C(devAddr_DES, 0x01, 0x01)
time.sleep(dwell_time)
port_status1 = board.ReadI2C(devAddr_DES, 0x4D,1)
logging.debug('Check RX_PORT_STS1 Register (0x4D): %s', hex(port_status1))
time.sleep(0.1)
logging.debug('port lock status: %s', hex(port_status1 & 0x01))
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E,1)
logging.debug('Check RX_PORT_STS2 Register (0x4E): %s', hex(port_status2))
time.sleep(0.1)
lock_status = 0
lock_sum = 0
for loop in range(0, 10, 1):
port_status1 = board.ReadI2C(devAddr_DES, 0x4D, 1)
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E, 1)
time.sleep(0.1)
if (((port_status1 & 0x3C) == 0) and ((port_status2 & 0x20) == 0)):
lock_sum += int(port_status1 & 0x01)
else:
board.ReadI2C(devAddr_DES, 0x56, 1) # clear parity error
time.sleep(0.1)
lock_avg = round(float(lock_sum) / 10, 2)
lock_str = "%0.1f" %lock_avg
logging.debug('port lock status: %s', lock_str)
time.sleep(0.1)
out_string = lock_str + ","
f1.write(out_string)
print lock_str
logging.debug('**cdly_ctrl value at end of loop**: %s', hex(cdly_ctrl))
cdly_ctrl = 8 #(disable 6 extra delay)
for ddly_ctrl in range(8, 16, 1):
# write reg_8
board.WriteI2C(devAddr_DES, 0xB2, ((ddly_ctrl<<4) + cdly_ctrl))
time.sleep(0.1)
logging.debug('**reg_8 updated value**: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
# reset digital block except registers
board.WriteI2C(devAddr_DES, 0x01, 0x01)
time.sleep(dwell_time)
port_status1 = board.ReadI2C(devAddr_DES, 0x4D,1)
logging.debug('Check RX_PORT_STS1 Register (0x4D): %s', hex(port_status1))
time.sleep(0.1)
logging.debug('port lock status: %s', hex(port_status1 & 0x01))
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E,1)
logging.debug('Check RX_PORT_STS2 Register (0x4E): %s', hex(port_status2))
time.sleep(0.1)
lock_status = 0
lock_sum = 0
for loop in range(0, 10, 1):
port_status1 = board.ReadI2C(devAddr_DES, 0x4D, 1)
time.sleep(0.1)
port_status2 = board.ReadI2C(devAddr_DES, 0x4E, 1)
time.sleep(0.1)
if (((port_status1 & 0x3C) == 0) and ((port_status2 & 0x20) == 0)):
lock_sum += int(port_status1 & 0x01)
else:
board.ReadI2C(devAddr_DES, 0x56, 1) # clear parity error
time.sleep(0.1)
lock_avg = round(float(lock_sum) / 10, 2)
lock_str = "%0.1f" %lock_avg
logging.debug('port lock status: %s', lock_str)
time.sleep(0.1)
out_string = lock_str + ","
f1.write(out_string)
print lock_str
# write reg_8 default value
board.WriteI2C(devAddr_DES, 0xB2, 0x0)
time.sleep(0.1)
#do a final digital reset including registers
board.WriteI2C(devAddr_DES, 0x01, 0x02)
time.sleep(0.1)
#readback RX_PORT_STS1 to clear Lock status changed on RX Port 0
board.ReadI2C(devAddr_DES, 0x4D, 1)
time.sleep(0.1)
logging.debug('reg_8 default value: %s', hex(board.ReadI2C(devAddr_DES, 0xB2)))
time.sleep(0.1)
logging.debug('DES lock & pass: %s', hex(board.ReadI2C(devAddr_DES, 0x04,1)))
time.sleep(0.1)
f1.close()
Best,
Zoe