Part Number: DS90UB924-Q1
Hi team,
It has been confirmed that the red line is generated in monitor on the customer side. This occur about 20 times in 6000 times by repeating the operation ON 4s to OFF 5s. The controller side is always on.
Ser/Des: 925/924
They changed Path-Through register 1 to 0(default), this problem was solved.
What effect does setting the Reserved flag to a value that is not a Default have on FPD link Ⅲ to OLDI conversion?

Is the Pixel clock edge setting in the register map of 926, but is the same set up/hold done during FPDLINK Ⅲ => OLDI conversion in the Reserved part of 924?

Regards,
Youhei MIYAOKA