Part Number: DS160PR421
Other Parts Discussed in Thread: DS160PR410
Hello,
For cost reason and easy supply management (single part to buy), we intend to use the DS160PR421 even where we do not need the mux function.
What to do with the unused inputs in this case?
Keep the pins unconnected?
These pins are internally biased due to the AC coupling, but is it allow and better to connect these pins to GND?
In the other hand, we will configure all the DS160PR410 through I2C to have a maximum flexibility (14 components managed with two I2C buses).
Can you confirm that the PD pin from all DS160PR410 can be permanently connected to GND?
The component does not need at least one high pulse on PD pin to always start up correctly (Rx detect state machine reset is in any case available through I2C Reg 0x0D bit3)?
Could you also confirm that we have no possibility to put some channels/all channels in standby through I2C (available on 75lvpe5421 but not on DS160PR421)?
Thank you for your help.
Regards
Michel Counson