Part Number: DS90UB960-Q1
Hi,
I would like to ask if I can work with the DS90UB960-Q1 at the next option-
CSI0 is transmiting the 960 test pattern
CSI1 is transmiting the input video from channel 0-3.
Thanks
Shmuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Hi,
I would like to ask if I can work with the DS90UB960-Q1 at the next option-
CSI0 is transmiting the 960 test pattern
CSI1 is transmiting the input video from channel 0-3.
Thanks
Shmuel
Hello Shmuel,
unfortunately, this is not supported. You can use either Camera inputs or Pattern Generator.
Hi,
Can I transmite the test pattern only to CSI1?
Can I transmite only channel 0 to CSI0?
Thanks
Hello Shmuel,
No, the test pattern must be generated on CSI0 and then can be replicated on CSI1.
Means, either you can work with test pattern or with incoming data over RX ports. You can't mix.
Hi Hamzeh,
So I can generate test pattern on CSI0 and transmite channel 0 to CS1?
Shmuel,
as I said, you can't mix between incoming signal and patgen signal. Also, this is something we never tested or validated, nor I have the ability to test.
Hello Shmuel,
I diged in further and have good news for you now.
If we choose not to replicate the contents of CSI_TX_PORT0 on CSI_TX_PORT1, the two ports work independently.
Patgen is connected to CSI_TX_PORT0 only and can be brought out on PORT1 through replication. Which means, yes, you should be able to have Patgen on CSI TX Port0, and the Camera (RX Port0) data on CSI TX Port1.
But as I said, we never tested or validated this use case, nor I have the ability to test