Part Number: SN65DSI83-Q1
Dear Expert,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI83-Q1
Dear Expert,
Thank you for the quick response,
We are using DSI_CLK.A0700WXF2MAAADB01 Preliminary Spec V1.2 (1) (1).pdfConfig.reg values.pdf
Attaching display panel spec and config. registers values.
Hey Krithika,
If possible try implementing a REF_CLK that meet the panel DClock Frequency of 62.23 MHz < f < 79.12 MHz. The REF_CLK will be a cleaner clock and may fix this sporadic issue. Additionally, is the DSI stream coming in with a clock of approx.185MHz? It looks like you're using the DSI_CLK-DIVIDER to divide the incoming clock speed by 3.
Thanks for the Feedback. Currently we don't have provision for REFCLK in our board and we will consider the implementation of a REF_CLK in the next revision. In the meantime, Can you suggest any solution that can be addressed through software? our DSI CLK currently measures approximately 200MHz. Please confirm that the configuration file shared is OK with respect to the Panel that we are using.
Hey Krithika,
The most important settings for sporadic issues like yours are register 0x0A, 0x0B, 0x10, and 0x12.
From your config:
LVDS_CLK: 62.5MHz - 87.5 MHz
DSI_CLK = 200MHz
2 lanes used
DSI_CLK_RANGE = 0x26
A good test would be to try to increase DSI clock to approx. 187.5 MHz, so its not on the edge of the range intervals (5 MHz). This would mean that the DSI_CLK_RAGE you want to use would be 185 - 190 MHz. If you change this but keep your divider the same the output LVDS clcok should be 62.5 Mhz. This would able put you closer to the nominal DCLK of your panel which is 62.58 MHz, which may get rid of your sporadic issue. This will put you at the edge of the LVDS clock frequency range, but its closer to your ideal panel spec.
If this doesn't work simply try to find a combination of DSI_CLK, and LVDS_CLK that meets spec, and isn't an edge case for any of the range registers.
Best,
Vishesh Pithadiya
Dear Vishesh,
We are using 4 lanes. We will change the DSI_CLK_RANGE to 185-190MHz.
Thanks and regards,
Krithika T
Let me know if you run into the same issues. If this doesn't fix the issue, the best route moving forward would be to implement a REF_CLK.