Part Number: DS125BR111
Hi Experts,
I use DS125BR111 on 3.3V mode, and I would ask a decoupling capacitor's value.
I look a datasheet and it is described "3.3V mode, decouple each VDD pin with 0.22uF cap to GND." in the Pin Functions table. On the other hand it is described "Place 0.1μF capacitors close to VDD Pins. Total capacitance should be ≦ 0.2 uF" in power Supply Recommendation. The description is different from each other. Which is correct? And if later one is correct, what will it occur with large capacitance exceeding 0.2uF.
Regards,
Tetsuya,