This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAL6408: How to read the command byte in the datasheet

Guru 14990 points

Part Number: TCAL6408
Other Parts Discussed in Thread: TCAL6416, TCA6408

Hi,

Command Byte is described in Table 7-4 of the data sheet.

When written in the command byte, it is "01h", but when written to the Output Port register, it is "02h".

In the configuration described in the command byte, it is "03h", but when written to the configuration register, it is "06h".

Both are written as if the bits are off. Could you please tell me which one is correct?

Thanks,

Conor