Part Number: DS90UB960-Q1
Hi,
I want to work with the following setup-

What the virtual ID I'll be at CSI1?
The test pattern (953) ID is VC3.
Thanks
Shmuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Hi,
I want to work with the following setup-

What the virtual ID I'll be at CSI1?
The test pattern (953) ID is VC3.
Thanks
Shmuel
Hello Shmuel,
You can re-assign the VC-ID as you want from 0 to 4. This can be done on DES reg 0x72
Hi,
This reg. over write the ID 3 from the 953?
So if the default of reg. 0x72 is e4 that means the csi1 vc is VC1.
The default settings in reg 0x72 is to keep the original VC. So, in your case VC3 will stay as VC3.
If you want to change that, this can be done in register 0x72.