Hi,
We are using DP83867 1G phy over RGMII with JETSON AGX orin and did following changes in dtsi. Please let me know it is correct or not-
ethernet@2310000 {
status = "okay";
nvidia,mac-addr-idx = <0>;
nvidia,max-platform-mtu = <8000>;
nvidia,pause_frames = <0>;
local-mac-adress = [1a 2b 3c 4d 5e 6f];
nvidia,phy-reset-gpio = <&tegra_main_gpio TEGRA234_MAIN_GPIO(G, 5) 0>;
phy-handle = <&phy>;
phy-mode = "rgmii-id";
mdio {
compatible = "ethernet-phy-ieee802.3-c22"; //THIS IS BASED ON WHAT WE READ
ON TI FORUM FOR THIS PHY
#address-cells = <1>;
#size-cells = <0>;
phy: phy@0 {
reg = <0>; // WE ARE NOT SURE IF 0 IS RIGHT ADDRESS, ADVICE ON HOW TO
CHECK WHAT ADDRESS WE UPDATE HERE
tx-fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
rx-fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,max-output-impedance;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_25_NS>;
ti,tx-internal-delay = <DP83867_RGMIIDCTL_2_75_NS>;
interrupt-parent = <&tegra_main_gpio>;
interrupts = <TEGRA234_MAIN_GPIO(G, 4) IRQ_TYPE_LEVEL_LOW>;
};
};
};
Thanks
Sagar