Part Number: XIO2001
Hello,
it seems that the XIO2001 requires a (single-ended) 125 MHz reference clock when used in a PCI Express Separate Refclk Architecture?
Am I getting it right: when the other/remote port device (e.g. a PCI Express Switch) requires a 100 MHz oscillator (or clock source) for PCI Express Separate Refclk Architecture then we just spend a 100 MHz oscillator on the other device REFCLK input and say a 125 MHz 100ppm oscillator on the XIO2001 REFCLK input and the PCI Express Link would work fine?
Thanks