This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3210 Self Power



Hello,

I found  #21 pin in TUSB3210 is Ground in the data sheet .

However,  #21 pin in the schematic  of the TUSB3210KBDPDK  user's guide, is "SELF/BUS" and

can be selected to 3.3V or GND.

Which is Correct?

We  want to use TUSB3210 with Self powered. ( 3.3V/5V is always On).

Best Regards

  • Hello,

    Datasheet is a little ambiguous,

    If you want the device to be always self powered, connect terminal 21 to 3.3V.

     

    Regards.

  • ELIAS san

    Thank you for your  reply.

    I am confused, because customer had already designed the Mass production as same as data sheet.

    When we use self powerd,  If #21pin of TUSB3210 were GND ( as same as DataSheet), what is the problem ?

    I could not find any   discription about  "self powered " , except page 28 section 2.6.4 "USB Control register"  in the Data Sheet.

    Would you please let me know more detail about #21pin ?

    There are no discription about #21(Ground? Self/Bus?)  in the Fig1-1 Block diagram also.

    Sorry to bother you again,

    Best Regards

  • Hello,

    If customer designed accordingly with the datasheet, everything should be ok.

    The problem here is that there are some ambiguous descriptions. The implementation guide talks about "self-powered" but does not identify if the self-power configuration is for the Evaluation Module or for the device itself.

    I am gathering information to   give you a better answer. Again, if they follow the datasheet it is OK.

     

    Regards.

  • Hello,

    I have confirmed that pin#21 should be tied to GND, this will not affect to your self-powered configuration.

    Regards.