This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: RBIAS Voltage

Part Number: DP83822I

Hello TI Team! I have some problems with DP83822IRHB, it couldn't work.

Section 2.4.2 (DP83822 Troubleshooting Guide) Probe the RBIAS pin says that: "Measure the DC value of the voltage across the RBIAS resistor and confirm that the voltage is 2.7 V."

Is this voltage correct? If the VDDA voltage is 1.8V, can the RBIAS voltage be 2.7V?

I measured the voltage equal to 1V, Rbias is exactly equal to 4.87kOhm 1%. (VDDA - 3.3V, VDDIO - 3.3V)

I doesn't have EVB to check this voltage. Could you check this?