This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDT100: Do you have any LVDS repeater which is newer device than SN65LVDT100?

Part Number: SN65LVDT100
Other Parts Discussed in Thread: DS25BR150, DS10BR150

Hello guys,

One of my customers use SN65LVDT100DGK for their current mass-productions.

But they are worry that EOL of this device would be EOLed in near future because this device developed in 2002.
So they is looking for any newer device which has same or similar function.
Do you have any recommended device?

Their signal frequency is 100MHz and transfer distance is less than 10 meters.

Thank you and best regards,
Kazuya.