Part Number: DP83TD510E
Hi,
I'm bothering you to ask for help with an issue. We have a board that includes TI's DP83TD510E Single Pair Ethernet Phy. We are having troubles while configuring it. It is connected to an SPE port with 10Base-T1L mode. Also it is connected to a ethernet switch with RGMII. And we are configuring it with a microcontroller on SMI bus. (Reg 0x3 of Phy returns 0x181.)
We want to connect 2 of these boards together over SPE ports. What should we do for auto-neg mode working? There is steps for master and slave configuring but we couldn't found any for auto-neg.
It is not communicating when we connect the 2 boards, then start ping from one PC to another (setup: PC1 -> board1 copper port (connected direclty to the switch fabric) -> board1 spe port (connected to dp83) -> board2 spe port -> board2 copper port -> PC2) we can see the simultaneus blinkings in the board1 copper port, board1 spe port and board2 spe port leds. It is vice versa if we start ping from PC2.
Also, we read 0x68 value from the reg 0x201, means there is no auto-neg link, bu we read 0x1 from the reg 0x10 means there is link.
What do you think the issue is? How can we configuring this phy when it is used under a switch fabric?
Best regards.