Part Number: TUSB8044AEVM
Other Parts Discussed in Thread: TUSB8044A
Hello there,
When I connect the TUSB8044AEVM to the USB-C port of the Surface Pro 7 laptop, a USB3 recognition error occurs in Windows. USB 2.0 operates normally, and there is no problem with USB3 recognition when connected to the USB-A port of the Surface Pro 7.
I have tested on two Surface Pro 7 laptops, and both are exhibiting the same symptoms.
Using the same cable with the TUSB8044AEVM, it works normally when connected to a MacBook Pro or Samsung Galaxy Book laptop.
Why is USB 3.0 not recognized only in the USB-C port of the Surface Pro 7?
I would appreciate any advice on what to look into.
Thanks
Sam