This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC813R-Q1: Field name

Part Number: DP83TC813R-Q1

Hi team,

I understand 0x11 bit[11] sgmii_soft_reset is setting for SGMII, so it is not a setting for RGMII.

Are there any register fields that apply to RGMII settings, even if the field name does not include rgmii, for example field name includes sgmii? 

Regards,

Youhei MIYAOKA

  • Hello Youhei,

    To my knowledge the only register that is related to RGMII settings but doesn't have RGMII in the name is this one:

    8.6.2.39 A2D_REG_48 Register (Address = 430h) [Reset = 0770h]

    This register is for configuring the TX and RX delay in RGMII mode. 

    Regards,

    Avtar