Part Number: TUSB320LAI
Hi team,
I am using TUSB320LAI with UFP.
Could you tell me the normal range of the CC waveform amplitude?
Or, if it is written in the specifications, could you tell me where it is written?
Best regards,
Yusuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB320LAI
Hi team,
I am using TUSB320LAI with UFP.
Could you tell me the normal range of the CC waveform amplitude?
Or, if it is written in the specifications, could you tell me where it is written?
Best regards,
Yusuke
Hi Yusuke,
Since you are configured for UFP, the CC lines should not exceed 2.04V at the maximum current value of 3A. This ensures that the 320 will detect the attached DFP. You can see this maximum voltage in the datasheet:

In CC negotiation, the DFP will hold both CC1 and CC2 at 5V. When a UFP is attached, the UFP presents pulldowns that lower the voltage on the CC lines to fall within a detection range (shown in the datasheet table). What voltage is present on the CC lines will depend on the current mode setting of the DFP.
Here is the table in the USB-C spec that defines this value as well.

Best,
Shane