This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX232E: Difference between MAX232E and MAX3232E

Part Number: MAX232E
Other Parts Discussed in Thread: MAX3232E

Hi,

May I know the difference between MAX232E and MAX3232E?

Could they be replacement for each other?

Thanks and Best regards,

Tiger

  • The MAX232E requires a 5 V supply; the MAX3232E also works with 3.3 V.

  • Hi Tiger,

    Clemens is correct //Thanks for the help//

    Another difference is the output swing on the cable driver side is wider in the 232 device (+/-7V) compared to the 3232 device(+/-5V typical).

    Absolute max is also slightly higher on the 232 device for input voltages at +/-30V.

    They can replace each other if you're okay with these differences. 

    -Bobby