Part Number: TS2PCIE412
Other Parts Discussed in Thread: TMUX1574, , TMUXHS4412
Hi,
- Would this kind of switching for the PCIe (gen 2) data lanes and control signals work ? The switches are not dynamically controlled, but bus is connected either-or to Endpoint1 or -2. After switching there will be handshaking through the bus. Idea is to use passive SPDT switches instead of a PCIe packet switch.
- TS2PCIE412RUAR is 4-CHANNEL 8:16 MULTIPLEXER/DEMULTIPLEXER PCI EXPRESS SWITCH
- TMUX1574 Low-Capacitance, 2:1 (SPDT) 4-Channel

Kind Regards,
Vesa S.