Part Number: DS160PT801X16EVM
Other Parts Discussed in Thread: DS160PT801
Hi,
I am going to use DS160PT801 re-timer for 2x4 bifurcation mode. Please let me know what will the combination for Lane0?
A_PET0 and A_PETR0- for TX
B_PET0 and B_PETR0 for RX
will create one lane(LANE0)
Please confirm, my understanding is correct or not?
Other Queries are-
1. If i am not using EEPROM then can we programmed it via SoC over I2C?
2. Since i am using it for backplane application which works on separate clock architecture, then what will be the termination require on lock
REFCLK+/- pins since it is input reference clock.
3. A Port and B port are interchangeable - means either port can be connect to SoC or back-plane?
Thanks
Sagar