Other Parts Discussed in Thread: TUSB2551A
I am currently working with the TUSB2551A USB transceiver and would like to ask for clarification regarding the need for external 15K ohm pulldown resistors in a downstream facing (USB host side) application. Although the spec sheet indicates that this part is USB 2.0 compliant, it is ambiguous as to whether the part has these 15K ohm pulldown resistors internally. On an upstream facing (USB client) application, these pulldown resistors should NOT be part of the circuit (you would only want the 1.5K pullup resistor which is configurable on this part through the SOFTCON line). The 15K ohm pulldown resistors, if they are there, do not seem to be configurable. I would like to better understand how this part can seemingly be used for both upstream facing port versus downstream facing port applications (if it can at all).